Flash Read Alignment Issue - Data Reads from 2n Instead of 2n+1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Read Alignment Issue - Data Reads from 2n Instead of 2n+1

Jump to solution
2,464 Views
zyz
Contributor III
Recently, when using the S32G274 M7 core to read data from flash, I encountered a forced alignment issue. When attempting to read data starting from an address 2n+1, the returned data starts from address 2n. However, reading from address 2n does not have this problem. We are bypassing FEE and directly using the FLS driver to operate the flash. The MCAL version is: SWS32G_RTD_4.4_4.0.2.
 
Who can help me, thank you.
0 Kudos
Reply
1 Solution
2,374 Views
zyz
Contributor III
Hi carlos_o,
Thank you for your support. I have already solved the problem on my side. This 2-byte alignment issue is caused by the inherent characteristics of FLASH and is not related to the software.

View solution in original post

0 Kudos
Reply
5 Replies
2,443 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @zyz,

Are you using a custom board? if not is it an RDB or EVB? 

If you are using a custom board, which model of QSPI are you using? 

The problem is when you are doing the bypass of the FEE driver and using directly the FLS? or this is a workaround? 

 

 

0 Kudos
Reply
2,433 Views
zyz
Contributor III

Hello carlos_o,

Yes, I am using our custom board with QSPI DDR mode. The flash model is MX25UW51245G.
 
I discovered this issue when directly using FLS.
0 Kudos
Reply
2,401 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @zyz 

I recommend try first with the IP functions instead of MCAL, you can see how it works at the Spi_Ip_Transfer example. Let me know if the issue persists. 

0 Kudos
Reply
2,375 Views
zyz
Contributor III
Hi carlos_o,
Thank you for your support. I have already solved the problem on my side. This 2-byte alignment issue is caused by the inherent characteristics of FLASH and is not related to the software.
0 Kudos
Reply
2,362 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @zyz, 

great to hear that. Let us know if there is anything we can do to help.

0 Kudos
Reply