Error while running assembler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error while running assembler

Jump to solution
3,280 Views
Bannai30
Contributor I

Hello I am currently trying to perform few tests and when I integrated the files in my project (tool used-IAR) it shows an error as below the path and the directory are correct and there is no mismatch. Can you tell me what is the possible reason for this error?

Thank you.

Bannai30_0-1657115898700.pngBannai30_0-1657115898700.png

 

Tags (1)
0 Kudos
Reply
1 Solution
3,263 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Bannai30,

 

You should contact IAR, since it works on our side.

 

Regards

View solution in original post

0 Kudos
Reply
2 Replies
2,901 Views
RachelGomez123
Contributor I

This fatal error is reported when a constant assembler expression performs a division by zero. These fatal error is reported when a constant assembler expression is too big to be evaluated by the constant parser. Try reducing the number of terms.

Regards,

Rachel Gomez

0 Kudos
Reply
3,264 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Bannai30,

 

You should contact IAR, since it works on our side.

 

Regards

0 Kudos
Reply