Error while running assembler

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error while running assembler

跳至解决方案
3,283 次查看
Bannai30
Contributor I

Hello I am currently trying to perform few tests and when I integrated the files in my project (tool used-IAR) it shows an error as below the path and the directory are correct and there is no mismatch. Can you tell me what is the possible reason for this error?

Thank you.

Bannai30_0-1657115898700.pngBannai30_0-1657115898700.png

 

标记 (1)
0 项奖励
回复
1 解答
3,266 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Bannai30,

 

You should contact IAR, since it works on our side.

 

Regards

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,904 次查看
RachelGomez123
Contributor I

This fatal error is reported when a constant assembler expression performs a division by zero. These fatal error is reported when a constant assembler expression is too big to be evaluated by the constant parser. Try reducing the number of terms.

Regards,

Rachel Gomez

0 项奖励
回复
3,267 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Bannai30,

 

You should contact IAR, since it works on our side.

 

Regards

0 项奖励
回复