Error while running assembler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error while running assembler

ソリューションへジャンプ
3,278件の閲覧回数
Bannai30
Contributor I

Hello I am currently trying to perform few tests and when I integrated the files in my project (tool used-IAR) it shows an error as below the path and the directory are correct and there is no mismatch. Can you tell me what is the possible reason for this error?

Thank you.

Bannai30_0-1657115898700.pngBannai30_0-1657115898700.png

 

タグ(1)
0 件の賞賛
返信
1 解決策
3,261件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Bannai30,

 

You should contact IAR, since it works on our side.

 

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,899件の閲覧回数
RachelGomez123
Contributor I

This fatal error is reported when a constant assembler expression performs a division by zero. These fatal error is reported when a constant assembler expression is too big to be evaluated by the constant parser. Try reducing the number of terms.

Regards,

Rachel Gomez

0 件の賞賛
返信
3,262件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Bannai30,

 

You should contact IAR, since it works on our side.

 

Regards

0 件の賞賛
返信