Enable LLCE support for Linux on S32G( Goldbox)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable LLCE support for Linux on S32G( Goldbox)

2,117件の閲覧回数
rital123
Contributor I

We would like to use CAN2ETH feature of LLCE. So need a few information on this:
1>Is this feature enabled for the same?It would be great if you can provide us with guide to use the existing CAN2ETH feature?
2>If No, please let us know how could it be done?
Are there any BSP changes to be done.

0 件の賞賛
返信
3 返答(返信)

1,815件の閲覧回数
salimmulla2021
Contributor III

@Bio_TICFSL 

Is LLCE supported on Linux operating system? If yes where we will get the BSP driver for same?

 

0 件の賞賛
返信

2,108件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello rital123,

 

You can view this appnote for reference:

https://www.nxp.com/docs/en/application-note/AN13423.pdf

 

regards

0 件の賞賛
返信

2,105件の閲覧回数
Aishwarya
Contributor I

@Bio_TICFSL 

CANtoETH process given in this pdf will be used for linux bsp installed Goldbox?

0 件の賞賛
返信