Enable LLCE support for Linux on S32G( Goldbox)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable LLCE support for Linux on S32G( Goldbox)

2,099 Views
rital123
Contributor I

We would like to use CAN2ETH feature of LLCE. So need a few information on this:
1>Is this feature enabled for the same?It would be great if you can provide us with guide to use the existing CAN2ETH feature?
2>If No, please let us know how could it be done?
Are there any BSP changes to be done.

0 Kudos
Reply
3 Replies

1,797 Views
salimmulla2021
Contributor III

@Bio_TICFSL 

Is LLCE supported on Linux operating system? If yes where we will get the BSP driver for same?

 

0 Kudos
Reply

2,090 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello rital123,

 

You can view this appnote for reference:

https://www.nxp.com/docs/en/application-note/AN13423.pdf

 

regards

0 Kudos
Reply

2,087 Views
Aishwarya
Contributor I

@Bio_TICFSL 

CANtoETH process given in this pdf will be used for linux bsp installed Goldbox?

0 Kudos
Reply