Docker Container on S32G399ardb3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Docker Container on S32G399ardb3

1,506 Views
ankitv
Contributor II

I am running Ubuntu 20.04 using Linux BSP 38.0 on Goldbox3

I see that even basic operations like copying a file or changing the permissions of a file are taking strangely too long - look at the last 2 lines of the image below

ankitv_0-1707253688855.png

A basic container of just Ubuntu 20.04 base and ROS2 Foxy base is taking more than 2minutes to start. htop commands shows all cores maxing out. 

ankitv_1-1707253906649.jpeg

 

Can you please advise what might be causing this and how to resolve this ? Thanks

-Ankit

0 Kudos
Reply
1 Reply

1,481 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Do you build the base ubuntu image? Or were there additional features enabled?

As for before executing the command, were there any additional commands that were executed? If so, which ones?

Can you share the full log of what you are seeing?

Please, let us know.

0 Kudos
Reply