Docker Container on S32G399ardb3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Docker Container on S32G399ardb3

1,501件の閲覧回数
ankitv
Contributor II

I am running Ubuntu 20.04 using Linux BSP 38.0 on Goldbox3

I see that even basic operations like copying a file or changing the permissions of a file are taking strangely too long - look at the last 2 lines of the image below

ankitv_0-1707253688855.pngankitv_0-1707253688855.png

A basic container of just Ubuntu 20.04 base and ROS2 Foxy base is taking more than 2minutes to start. htop commands shows all cores maxing out. 

ankitv_1-1707253906649.jpegankitv_1-1707253906649.jpeg

 

Can you please advise what might be causing this and how to resolve this ? Thanks

-Ankit

0 件の賞賛
返信
1 返信

1,476件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Do you build the base ubuntu image? Or were there additional features enabled?

As for before executing the command, were there any additional commands that were executed? If so, which ones?

Can you share the full log of what you are seeing?

Please, let us know.

0 件の賞賛
返信