Hi,
I am working on Developing the UART Driver for LLCE,
i have few doubts with respect to the LLCE, i have installed LLCE Package in the s32 design studio and i have installed the .exe file also, so i get example of LIN, CAN, SPI,FLEXRAY in the Package.
in LIN example, it seen that there is function called llce_firmware_load which loads the LLCE enablement bin releases to the SRAM memory.
in case if i am developing my own driver for UART in LLCE, is it needed to load the binary given in example to my project as well?
@Daniel-Aguirre#LLCE #S32G274A
Using LLCE as UART in S32G2RM
@bpe
and regarding the UART Driver,
if i am accessing the LINflexD registers in LLCE for UART configuration, we have BDRL registers for data transfer,
will it be okay to use the same for data transfer, or else i need to use the FIFO available in LLCE