Developing UART driver in LLCE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Developing UART driver in LLCE

跳至解决方案
2,163 次查看
Naveenkumar_Muthusamy
Contributor IV

Hi,

I am working on Developing the UART Driver for LLCE, 

i have few doubts with respect to the LLCE, i have installed LLCE Package in the s32 design studio and i have installed the .exe file also, so i get example of LIN, CAN, SPI,FLEXRAY in the Package.

in LIN example, it seen that there is function called llce_firmware_load which loads the LLCE enablement bin releases to the SRAM memory.

in case if i am developing my own driver for UART in LLCE, is it needed to load the binary given in example to my project as well?

@Daniel-Aguirre#LLCE #S32G274A

Using LLCE as UART in S32G2RM 

@bpe 

and regarding the UART Driver, 

if i am accessing the LINflexD registers in LLCE for UART configuration, we have BDRL registers for data transfer,

will it be okay to use the same for data transfer, or else i need to use the FIFO available in LLCE

标记 (4)
0 项奖励
回复
1 解答
2,152 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We have answered through the internal channel.

Have a great day.

在原帖中查看解决方案

1 回复
2,153 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We have answered through the internal channel.

Have a great day.