Debug M7 with probe while Linux is running on A53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug M7 with probe while Linux is running on A53

969件の閲覧回数
curiousmindflow
Contributor II

Hello,

How can i debug a binary launched on the M7 cortex with the S32 debug probe while Linux is running on the A53 ?

タグ(1)
0 件の賞賛
返信
1 返信

955件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

You can debug an image previously loaded to external flash by following the pages 11 and 12 of the following document:

"C:/nxp/S32DS.3.4/S32DS/help/resources/howto/gdev/HOWTO_JTAG_flash_programming_with_S32_Debugger_and_S32_Debug_Probe_for_S32G274A_EVB.pdf"

This resource should be provided by installing S32DS. In the said pages, there are a few steps that you need to follow in order to debug a running program.

Please, let us know if this information was helpful or not.

0 件の賞賛
返信