Debug M7 with probe while Linux is running on A53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug M7 with probe while Linux is running on A53

1,349 Views
curiousmindflow
Contributor II

Hello,

How can i debug a binary launched on the M7 cortex with the S32 debug probe while Linux is running on the A53 ?

Tags (1)
0 Kudos
Reply
1 Reply

1,335 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

You can debug an image previously loaded to external flash by following the pages 11 and 12 of the following document:

"C:/nxp/S32DS.3.4/S32DS/help/resources/howto/gdev/HOWTO_JTAG_flash_programming_with_S32_Debugger_and_S32_Debug_Probe_for_S32G274A_EVB.pdf"

This resource should be provided by installing S32DS. In the said pages, there are a few steps that you need to follow in order to debug a running program.

Please, let us know if this information was helpful or not.

0 Kudos
Reply