Cannot wake up from RTC0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot wake up from RTC0

1,509件の閲覧回数
Jeff-CF-Huang
Contributor III

Hi Sir,

I run the below command to try suspend/resume function.

 

echo;date;echo; rtcwake -d rtc0 -m mem -s 180; echo;date

 

My board can suspend successfully, but it cannot wake up after 180 seconds.

In contrast, the RDB3 is able to perform this function.

Could you share some experiences on how to investigate why my board is unable to do so?

 

Best regards,

Jeff Huang

0 件の賞賛
返信
4 返答(返信)

1,454件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hi, @Jeff-CF-Huang 

Thanks for your reply.

Since the system could resume by other wakeup resource, it is possibly no issues on suspend process, would you please help to rebuild the TFA adding these parameters"S32_USE_LINFLEX_IN_BL31=1 DEBUG=1"

Disable the PFE, then test it again, we can continue supporting it with the logs shared.

 

BR

Chenyin

0 件の賞賛
返信

1,457件の閲覧回数
Jeff-CF-Huang
Contributor III

Hi Chenyin,

We are developing our product based on BSP40. It can be awakened by an external RTC (RTC1) or by other GPIOs.

During our suspend/resume tests, we observed that RTC0 continues counting while the system is suspended.

Therefore, we believe the issue may reside in the wake-up source configuration.

Best regards,

Jeff Huang

0 件の賞賛
返信

1,486件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Jeff-CF-Huang 

Furthermore, would you help to share the full log of STR test on your custom board?(from boot up to the end)

Sometimes, maybe the board stopped at certain phases while entering the suspend, thus could be resumed.

 

BR

Chenyin

0 件の賞賛
返信

1,489件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Jeff-CF-Huang 

Thanks for your post.

Would you mind sharing more information regarding to the issue, Which version of BSP is used during the test? 

BR

Chenyin

 

0 件の賞賛
返信