Can_43_LLCE "postBuildVariantUsed" Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can_43_LLCE "postBuildVariantUsed" Error

2,356 Views
Archieeeee
Contributor II

LLCE  Version :S32G_LLCE_1_0_7

RTD Version:  SW32G_RTD_4.4_4.0.2_HF02

EB Version : 27.1

使用LLCE Demo :sample_app_can_llce\tresos_s32g2\Tresos_CAN2CAN_Project

Can Demo :Can_TS_T40D11M40I2R0\examples\EBT\S32G2\Can_example_S32G274A_M7

Spi Demo:  Spi_Transfer_S32G274A_M7\TresosProject\Spi_Transfer_S32G274A_M7

三个工程的xdm 文件,合成一个新的工程,LLCE 报错如下

 

category : Error
project : OpenVoc_McalProject
description: A node may only have selectable variation points defined in case the "postBuildVariantUsed" parameter at the module definition is set to true.
Either remove the variation point at this parameter or enable the mentioned boolean parameter.
detailed : A node may only have selectable variation points defined in case the "postBuildVariantUsed" parameter at the module definition is set to true.
Either remove the variation point at this parameter or enable the mentioned boolean parameter.
id : 95035
resource :
path : /AUTOSAR/TOP-LEVEL-PACKAGES/Can_43_LLCE/ELEMENTS/Can/CanConfigSet/CanHardwareObject/CanHardwareObject_0/CanIdType
location :
stack :

 

 

image.png

 

EcucPostBuildVariants:

image.png

 

Pls Help

0 Kudos
Reply
4 Replies

2,344 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you help us translate your inquiry to English? We understand that you are combining 3 examples, but we would like confirmation on this.

If our assumption is correct, care should be taken to merge different examples. Are you seeing any errors under the independent examples? Is this only happening under the 3 examples merging? Or when an specific combination is happening (i.e. LLCE+CAN or CAN+SPI or LLCE+SPI)?

Under the public community, we don't commonly provide support on merging examples or mayor modifications, but we will provide as much support as we can offer.

Please, let us know.

0 Kudos
Reply

2,339 Views
Archieeeee
Contributor II

Hi  Daniel:

Thanks for your reply; no error  under any independent examples; I Meged the three example:  sample_app_can_llce+Can_example_S32G274A_M7+Spi_Transfer_S32G274A_M7   by 3 step

step 1: merge Can_example_S32G274A_M7+Spi_Transfer_S32G274A_M7  it's work ok

step 2: copy Can_43_LLCE.xdm (sample_app_can_llce) to my project 

step 3: add Dio Ipcf Module,and config it manual

How should I fix this error

0 Kudos
Reply

2,335 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for the information.

We understand that you are also adding additional modules aside from the 3 examples (step 3). Prior to this step, after step 2 are you seeing any problems?

We mean that if step 1 + step 2 works OK. For us to understand if the issue is related to the 3 examples being merged, or to the additional modules.

Please, let us know.

0 Kudos
Reply

2,259 Views
Archieeeee
Contributor II

Hi, Daniel:

 Thanks for you reply; i sloved this issue by enable CAN->Gernnal  Post Build Variant Used ;

Thank you !

BR

0 Kudos
Reply