CAN2ETH build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN2ETH build error

2,895 Views
seeu
Contributor III

dear nxp experts:

I follow the file AN13424 Using CAN2CAN, CAN2ETH and ETH2CAN
Features of LLCE on S32G
 ,
after all step finish, I try to use 'make' command to build,but it occur error,how to solve this problem? please refer to the attachment,thank!

Tags (1)
0 Kudos
Reply
3 Replies

2,861 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

It seems there is a ticket for this same request under the NXP online services, is this correct?

Please, let us know.

0 Kudos
Reply

2,841 Views
seeu
Contributor III

yes,it is me.Now I can built it sucessful, but I connect CAN wire between CAN0 and 1, Also connect Ethernet cable to PA3(my board is S32G274aRDB2), and run the script "s32g.cmm",wireshark capture nothing, and I use CANalyst to capture the CAN0 and CAN1(the baudrate is 500kbps/2Mbps),also get nothing.

0 Kudos
Reply

2,876 Views
seeu
Contributor III
 
0 Kudos
Reply