CAN Gateway Slow Path

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN Gateway Slow Path

1,435 Views
akhil_k_appu
Contributor III

For running the Cortex-M7 slow-path use cases, we set the  SW12 in ON-ON position. After this we need to run the  A53 slow-path use cases.

Is it required to make SW12 in ON-OFF Position ??

0 Kudos
Reply
2 Replies

1,424 Views
gmocanu
NXP Employee
NXP Employee

Hello,

 

You can keep SW12 in ON-ON position. This configuration is needed only to load a custom FW and switch table on SJA that are required for the cloud connectivity use case, and the M7-core-based routing. The other use cases / demos are not affected by this configuration.

 

Best regards,

George

0 Kudos
Reply

1,417 Views
akhil_k_appu
Contributor III

Thank you @gmocanu 

0 Kudos
Reply