CAN Driver on M7, LLCE interfaces not selectable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN Driver on M7, LLCE interfaces not selectable

1,876件の閲覧回数
DasKeks
Contributor II

I'm trying to setup the CAN drivers in a project for the M7 cores. I added a project in the S32 design Studio. I tried to add the CAN driver under the peripherals section, but I can only select the FLEXCAN interfaces.

Is there a driver for the other (LLCE) CAN interfaces? Or how can I add the RTD driver for these interfaces?

0 件の賞賛
返信
1 返信

1,849件の閲覧回数
asap
NXP Employee
NXP Employee

hi nxp19,

LLCE drive+firmware has been listed under S32G standard software category, please refer to related product brief or open Automotive software package manager to download all the software deliverables. 

furthermore, you may want to visit the S32G training acadmy - advanced training for S32G2 processor:

Albert
0 件の賞賛
返信