Building Real Time Bootloader from GoldVIP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Building Real Time Bootloader from GoldVIP

2,652 次查看
s153022
Contributor III

Hello NXP Support,

I am trying to build the Real Time Bootloader (Bootloader_S32G3XX_ASR_4.4_M7) in EB Tresos following the Bootloader-User_Manual.pdf in GoldVIP-S32G3-1.11.0.

On page 18, it instructs to:

  1. Import the bootloader project from GoldVIP_install_path\realtime\s32g399ardb3\bootloader\workspace\Bootloader_S32G3XX_ASR_4.4_M7
    • Select File -> Import.
    • Search for Existing Projects into Workspace option and click on Next.
    • Choose Select root directory, then click Browse button and add the above mentioned workspace.

I have successfully imported the project following these steps. However, I encountered an issue when trying to Load Configuration by right-clicking on the imported project. 

 

contributor3_0-1717481797297.png

The specific problem I am facing is shown in below screenshot.

contributor3_1-1717481906898.png

Could you please provide guidance on how to resolve this issue?

Thank you in advance for your assistance.

0 项奖励
回复
5 回复数

2,636 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

These errors are related to EB Tresos not finding the corresponding modules. Have you copied the plugins available under the Bootloader > eclipse folder? These are shown below:

DanielAguirre_0-1717507043824.png

Once you copy them, you need to restart EB Tresos, since they will not be taken into account until EB Tresos has been restarted.

Please, let us know.

0 项奖励
回复

2,620 次查看
s153022
Contributor III

Thank you,

I copied the plugins available under the Bootloader > eclipse folder, and re-started EB Tresos.

Some issues have been fixed  

But now I see the following three errors:

 

sami153022_0-1717556034486.png

 

Could you please suggest how to fix these as well?

 

Thanks and Best Regards

0 项奖励
回复

2,611 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

These plugins are related to the SAF or SDP packages from NXP. If you do not have any of those available, you should be able to remove them from that same window and continue without SAF/SPD support.

If you are looking into using them, you should also add the SAF/SPD plugins to your plugins folder of Tresos.

Please, let us know.

0 项奖励
回复

2,605 次查看
s153022
Contributor III

Thanks for quick reply,

I've installed the S32G_SPD_2.0.0, and I can see the following plugins installed in the SPD folder below.

sami153022_1-1717639438953.png

 

 

However when I load configuration in the EB tresos, I get below errors again.

sami153022_0-1717639416171.png

Is this part of SAF package? where can I get SAF package?

Best Regards

0 项奖励
回复

2,582 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. That is correct. The modules that are still missing are related to the SAF package.

If you are looking into using SAF, then help us contacting your local NXP FAE/DFAE/representative, since it is a premium package.

Please, let us know.

0 项奖励
回复