Hello,
For a robotic project i need to run a Linux on the cortex A53 and a FreeRTOS on the cortex M7, both simultaneously.
Can someone point me to the good direction please ?
In advance, thank you 
解決済! 解決策の投稿を見る。
There is a demo for this boot scenario, however, it currently requires a download approval. I will contact you by e-Mail with more information.
Best Regards,
Platon
Where can I download the software? And how does different core access the peripheral? I assume there is one set of peripheral for the single chip.
There is a demo for this boot scenario, however, it currently requires a download approval. I will contact you by e-Mail with more information.
Best Regards,
Platon
Can you share this demo with me too please?
I would like access to this example as well. I plan to run Yocto for the A cores and Zephyr RTOS on the M core.
Hello, Could I get such an example forwared to me as well? I've opened a support ticket about this too
Can you share me me as well?
How can I access this demo? can you please provide access
for S32G multicore (A53 and M7) boot demos, some published resources listed here:
1. GoldVIP - Boot and Partitioning (Automotive Software package manager- S32G2 - bundles and use cases - GoldVIP, once installed, refer to User Manuel chapter 4.2 deploy goldvip images and chapter 6. boot flow; and Developer's guide chapter 2.1 & 2.2), when you read the documentation, you can also refer to the video clips on GoldVIP traing academy - GoldVIP Get started
2. NXP reference software - Integration reference examples (Automotive Software package manager- S32G2 - bundles and use cases - Integration reference examples, once installed refer to documentation->release note and user manuals)
3. S32G2 traning academy - S32G2 boot overview
4. "Enabling Multicore application on S32G2 using S32G2 platform software integration - application note" : AN17350 (also provided associated AN13750SW)
5. "Automotive premium engineering service" : https://www.nxp.com/support/support/nxp-engineering-services/automotive-premium-services:AP-PREMIUM-..., you could find professional automotive engineering services/training offering from here.
6. contact your NXP local sales to seek further help.
hope that helps.
Hi NXP employee,
We treid all the links, those are not help full. Please dont deviate the topic. Please go the nxp reply above and share the solutions. we are dieing and digging the codes every thing wat not to say.
NXP Gold VIP is working fine but NXP example demo codes are not working. This NXP is intentionally hidding the information. How we can progress here A53 and M7 to load.
Regards,
Viswanath K
hi viswa_kondapall,
I have just updated my post to include two recent update regarding the collatoral/demo software we provided for customer reference. please understand booting and multicore booting are deep technical projects especially the complex multicore system like S32G. in this open community, we can provide the best effort with our technical team also community experts to give high level guides, explain the offer we provided also prepare further chance to follow up with customer offline. Please contact your local sales/fae representative to initiate that discussion
thank you for your understanding
Hi
I also have the same demand. Can you expand this download method to me?
Hi,
Can you please give me access to this solution too.
Thanks.
Can you email me the demo app?
Hi NXP
I also have the same demand. Can you expand this download method to me?
Hello,
I finally succeeded to boot both at the same time.
Can you share me me as well?How can you find it?Thank you very much.I can send some e-books
to you!
@curiousmindflowwould you be okay to share the details here so others can benefit?