Boot A core and M Core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot A core and M Core

702 Views
Karthik_7
Contributor IV

Hello , 
How can I Boot A core and M Core where BSP is loaded to eMMC and Bootloader, AUTOSAR BSW package loaded to Nor flash,  What all Switch configuration i need to do and what all other configuration i need to do , to achieve this. 

Labels (1)
0 Kudos
Reply
1 Reply

677 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Karthik_7

Thanks for the question.

Generally, for your issues, I suggest referencing the AN13750, which could be downloaded from the S32G product page.

A bootloader is created,  which could boot the A53 cores with BSPs, and also boot the M7 core with your specific application image. Seems it could fulfill your requirements based on the example shown in this document.

Hope it helps

 

Best Regards

Chenyin

0 Kudos
Reply