Boot A core and M Core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot A core and M Core

1,143件の閲覧回数
Karthik_7
Contributor IV

Hello , 
How can I Boot A core and M Core where BSP is loaded to eMMC and Bootloader, AUTOSAR BSW package loaded to Nor flash,  What all Switch configuration i need to do and what all other configuration i need to do , to achieve this. 

ラベル(1)
0 件の賞賛
返信
1 返信

1,118件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Karthik_7

Thanks for the question.

Generally, for your issues, I suggest referencing the AN13750, which could be downloaded from the S32G product page.

A bootloader is created,  which could boot the A53 cores with BSPs, and also boot the M7 core with your specific application image. Seems it could fulfill your requirements based on the example shown in this document.

Hope it helps

 

Best Regards

Chenyin

0 件の賞賛
返信