Assistance Required for Configuring LIN over UART (Master/Slave Mode) on S32G3-VNP-RDB3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Assistance Required for Configuring LIN over UART (Master/Slave Mode) on S32G3-VNP-RDB3

917件の閲覧回数
P_lavanya18
Contributor I

 

We are currently working on enabling and testing LIN communication over UART on the S32G-VNP-RDB3 board running BSP . Our goal is to configure the board as a LIN slave /Master and verify communication using CANalyzer as the LIN master/Slave.

From the Linux user space, we have identified the following LIN-related UART devices:

  • FLEX_LIN: /dev/ttyLF2
  • LLCE_LIN: /dev/ttyLF3, /dev/ttyLF4, /dev/ttyLF5, /dev/ttyLF6

We are able to send data from the board to CANalyzer, but CANalyzer reports errors such as:

  • Invalid Header
  • Slow Response
  • Receive Error

 

タグ(4)
0 件の賞賛
返信
1 返信

865件の閲覧回数
carlos_o
NXP TechSupport
NXP TechSupport

Hi @P_lavanya18 

Thanks for your post.

Could you please provide how are you doing the configuration to set the transmission? 

Which BSP version are you using?

 

0 件の賞賛
返信