Add Functionality to SW1 in S32grdb2 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Add Functionality to SW1 in S32grdb2 board

跳至解决方案
2,091 次查看
athul_am
Contributor II

Hi,

I have a Requirement to add a custom functionality to a switch press in the s32grdb2 board, I would like to catch the button of the switch next to the Reset button labeled SW1.

I am not able to find the GPIO of that switch, if i can get the diagram for the PIN configurations that would be great.

Also I am doing this for the first time so if anyone can provide a reference of any such implementations that would be great.

Thanks in Advance,

Athul

 

标记 (1)
0 项奖励
回复
1 解答
2,075 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For what we are able to see under the RDB2 schematic (rev E), we understand that there is no direct user button under the board to add custom functionality. The SW1 you are referring to is linked to the POR (Power-On Reset) functionality of the S32G274A, as shown below:

DanielAguirre_0-1708440171911.pngDanielAguirre_0-1708440171911.png

We do apologize.

Please, let us know.

在原帖中查看解决方案

3 回复数
2,074 次查看
athul_am
Contributor II

Hi @Daniel-Aguirre ,

Thank you for the Response, so there is no switch or button in the board to add a customizable functionality to it ,is my understanding correct.

 

0 项奖励
回复
2,069 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For what we are able to see, this is correct.

Please, let us know.

0 项奖励
回复
2,076 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For what we are able to see under the RDB2 schematic (rev E), we understand that there is no direct user button under the board to add custom functionality. The SW1 you are referring to is linked to the POR (Power-On Reset) functionality of the S32G274A, as shown below:

DanielAguirre_0-1708440171911.pngDanielAguirre_0-1708440171911.png

We do apologize.

Please, let us know.