s32 sonycam focal length

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32 sonycam focal length

1,338 次查看
alan13341313
Contributor I

What is the focal length of it ?

I can't find answer in datasheet

0 项奖励
回复
2 回复数

1,231 次查看
andrei_skok
NXP Employee
NXP Employee

The focal length of the S32V-SONYCAM is 6,1 mm

0 项奖励
回复

1,231 次查看
fangyue
Contributor II

Hi Andrei.,

Is the focal length the same for both x-axis and y-axis? Could you also tell me the principal point and image size of S32V-SONYCAM? I need these calibration parameters for further development. Thanks in advacne.

BR,

Yue

0 项奖励
回复