s32 sonycam focal length

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32 sonycam focal length

1,336件の閲覧回数
alan13341313
Contributor I

What is the focal length of it ?

I can't find answer in datasheet

0 件の賞賛
返信
2 返答(返信)

1,229件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

The focal length of the S32V-SONYCAM is 6,1 mm

0 件の賞賛
返信

1,229件の閲覧回数
fangyue
Contributor II

Hi Andrei.,

Is the focal length the same for both x-axis and y-axis? Could you also tell me the principal point and image size of S32V-SONYCAM? I need these calibration parameters for further development. Thanks in advacne.

BR,

Yue

0 件の賞賛
返信