pwm generation in S32K144

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

pwm generation in S32K144

1,326 次查看
harish_073024_
Contributor I

Hello team

we are using S32k144 uC in our designs. we currently preparing schematics. we need some clarification in uC ADC and FTM module. 

1. we are planning to generate the PWM 16khz with 75% duty cycle using FTM modules. But we need this PWM signal when the ADC pin detects 4V.

is it possible in this uC? if it is possible can tell me how to configure this one inside the uC??

标签 (1)
0 项奖励
回复
2 回复数

1,273 次查看
harish_073024_
Contributor I

thank for clarification.

we are using for generating the PWM using pin 39 FTM0_CH7 and pin 48 FTM3_CH0 (64 pin package).

1.FTM0_CH7 channel PWM is complementary type, is it possible to invert the output signal from this pin??

2.what is default FTM signals outputs, when there is PWM generation?

3.what is the difference between FTMx_CHx vs FTMx_FLTx??

0 项奖励
回复

1,294 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

The FTM hardware trigger source can be from many other modules via TRGMUX, like LPIT,
Low Power Timer, CMP, etc.

In your case, what you need to do is a configuration of CMP->TRGMUX->FTM.

Hope it helps you.

Have a nice day!

0 项奖励
回复