mpc5748G SDK compiler errors and warnings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mpc5748G SDK compiler errors and warnings

ソリューションへジャンプ
5,059件の閲覧回数
leonggz
Contributor II

Hello, i'm trying to import from an example project (flexcan_mpc5748g) using the SDK for 5847G. it seems i would need to do two extra steps before i can compile: 1, attach the SDK after import is completed; 2, generate code from ProcExpert. 

this seems to work if i try to build right after the code gen from procExpert except a few warnings about non-existance path in the SDK, for example:

Description Resource Path Location Type
Invalid project path: Include path not found (C:\NXP\S32DS_Power_v1.2\S32DS\S32_SDK_MPC574xx_EAR_0.8.1\platform\pal\inc). flexcan_mpc5748g pathentry Path Entry Problem

Description Resource Path Location Type
Invalid project path: Missing project folder or file: \flexcan_mpc5748g\MPC5748G_SDK_Z4_0_GCC for Source path. flexcan_mpc5748g pathentry Path Entry Problem

while i was trying to follow the link, the mentioned pal\inc path indeed does not exist. while i was exploring around the generated sdk code (note this is after the .elf has been generated for the project), some code from the sdk starts to show red marks complaining "type bool could not be resolved". for example, in the clock_manager.c

status_t CLOCK_SYS_UpdateConfiguration(uint8_t targetConfigIndex,
clock_manager_policy_t policy)
{
uint8_t callbackIdx;
bool successfulSetConfig;

this would prevent me from any further rebuild of the same project.

so my question is two folds: 1, why i could build the project in the first place and generated the proj.elf? was there precompiled files from proc expert being copied to my proj folder? 2, what was the compiler settings or language settings that causes the bool type error? C99 defines bool but not C89/90 i guess.

thanks.

regards

gzhang

ラベル(1)
0 件の賞賛
返信
1 解決策
4,227件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

SDK guys updated little bit directory structure and forgot update some examples. In next release will be path removed. You can remove the include path by yourself from greened out options in project properties:


pastedImage_1.png

Jiri

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,227件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hello, 

thanks for report - I can reproduce the behavior. So - about your questions:

When you switch back from 89/90 dialect to 99 dialect - you can see errors about bool type. But if you check the console output - the .elf file is properly generated. The false-positive errors are caused by Eclipse Indexer. You can right click on project -> Index -> Rebuild and the bool "errors" will disappear. 


pastedImage_1.png

2. Yes - in 89/90 dialect is not bool type present and switching back to C99 without Index rebuild shows errors related to bool type. But project itself is compiled successfully.   

Jiri 

0 件の賞賛
返信
4,227件の閲覧回数
leonggz
Contributor II

Thanks for the confirmation, Jiri

can you check the missing directory warning as well? it's a warning only but every time i click on the SDK menu there is a popup trying to add those paths back. our project would require 'warning free' from the compiler.

thanks

regards

gzhang

0 件の賞賛
返信
4,228件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

SDK guys updated little bit directory structure and forgot update some examples. In next release will be path removed. You can remove the include path by yourself from greened out options in project properties:


pastedImage_1.png

Jiri

0 件の賞賛
返信