What's the difference between Bootloader_R45_M7_0 and Bootloader_S32R45_ASR_4.4_M7 for S32R45

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What's the difference between Bootloader_R45_M7_0 and Bootloader_S32R45_ASR_4.4_M7 for S32R45

Jump to solution
2,358 Views
aiweixin
Contributor IV

Hi,

    I install PlatformSoftwareIntegration_S32R45_2022_03_updatesite.zip in S32DS, and it generates "Bootloader_R45_M7_0" project.

aiweixin_0-1668764695948.pngaiweixin_0-1668764695948.png

    Then, i install Platform_Software_Integration_S32R45_2022_03.exe, and it generates "Bootloader_S32R45_ASR_4.4_M7" project.

aiweixin_1-1668764925045.pngaiweixin_1-1668764925045.png

    What's the difference between between the two projects? Whether there is dependency between them? or independent?

    The userManual doc of them seem the same absolutely.

    

Labels (1)
0 Kudos
Reply
1 Solution
2,346 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

first one is the project to be used/configured within S32 Design Studio, while the second one using Tresos studio.
Read chapter 6.1 Configuration of the bootloader user manual how to import/configure bootloaders example in selected tools.

BR, Petr 

View solution in original post

0 Kudos
Reply
2 Replies
2,347 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

first one is the project to be used/configured within S32 Design Studio, while the second one using Tresos studio.
Read chapter 6.1 Configuration of the bootloader user manual how to import/configure bootloaders example in selected tools.

BR, Petr 

0 Kudos
Reply
2,296 Views
aiweixin
Contributor IV

Thank you for your help.

0 Kudos
Reply