What's the difference between Bootloader_R45_M7_0 and Bootloader_S32R45_ASR_4.4_M7 for S32R45

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What's the difference between Bootloader_R45_M7_0 and Bootloader_S32R45_ASR_4.4_M7 for S32R45

ソリューションへジャンプ
2,388件の閲覧回数
aiweixin
Contributor IV

Hi,

    I install PlatformSoftwareIntegration_S32R45_2022_03_updatesite.zip in S32DS, and it generates "Bootloader_R45_M7_0" project.

aiweixin_0-1668764695948.png

    Then, i install Platform_Software_Integration_S32R45_2022_03.exe, and it generates "Bootloader_S32R45_ASR_4.4_M7" project.

aiweixin_1-1668764925045.png

    What's the difference between between the two projects? Whether there is dependency between them? or independent?

    The userManual doc of them seem the same absolutely.

    

ラベル(1)
0 件の賞賛
返信
1 解決策
2,376件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

first one is the project to be used/configured within S32 Design Studio, while the second one using Tresos studio.
Read chapter 6.1 Configuration of the bootloader user manual how to import/configure bootloaders example in selected tools.

BR, Petr 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,377件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

first one is the project to be used/configured within S32 Design Studio, while the second one using Tresos studio.
Read chapter 6.1 Configuration of the bootloader user manual how to import/configure bootloaders example in selected tools.

BR, Petr 

0 件の賞賛
返信
2,326件の閲覧回数
aiweixin
Contributor IV

Thank you for your help.

0 件の賞賛
返信