What's the difference between Bootloader_R45_M7_0 and Bootloader_S32R45_ASR_4.4_M7 for S32R45

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What's the difference between Bootloader_R45_M7_0 and Bootloader_S32R45_ASR_4.4_M7 for S32R45

跳至解决方案
2,331 次查看
aiweixin
Contributor IV

Hi,

    I install PlatformSoftwareIntegration_S32R45_2022_03_updatesite.zip in S32DS, and it generates "Bootloader_R45_M7_0" project.

aiweixin_0-1668764695948.pngaiweixin_0-1668764695948.png

    Then, i install Platform_Software_Integration_S32R45_2022_03.exe, and it generates "Bootloader_S32R45_ASR_4.4_M7" project.

aiweixin_1-1668764925045.pngaiweixin_1-1668764925045.png

    What's the difference between between the two projects? Whether there is dependency between them? or independent?

    The userManual doc of them seem the same absolutely.

    

标签 (1)
0 项奖励
回复
1 解答
2,319 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

first one is the project to be used/configured within S32 Design Studio, while the second one using Tresos studio.
Read chapter 6.1 Configuration of the bootloader user manual how to import/configure bootloaders example in selected tools.

BR, Petr 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,320 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

first one is the project to be used/configured within S32 Design Studio, while the second one using Tresos studio.
Read chapter 6.1 Configuration of the bootloader user manual how to import/configure bootloaders example in selected tools.

BR, Petr 

0 项奖励
回复
2,269 次查看
aiweixin
Contributor IV

Thank you for your help.

0 项奖励
回复