Hi Jiri,
when I use this workaround the components are use the “old” repository.
I want to use the new SDK with the old configurations from the components.
I tried to change the repository for the components separate, but then then configuration in the components changed.
Question:
At which time the files from the repository are copied to the project SDK path?
Where can I find the sCST lib ?
Lutz
Von: jiri.kral@nxp.com
Gesendet: Dienstag, 19. Dezember 2017 14:37
An: Köhler, Lutz <lutz.koehler@acd-antriebstechnik.de>
Betreff: Re: - Re: Update SDK in a S32DS project
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: Update SDK in a S32DS project
reply from Jiri Kral<https://community.nxp.com/people/jiri.kral@nxp.com?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/971279?commentID=971279&et=watches.email.thread#comment-971279>