Update SDK in a S32DS project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Update SDK in a S32DS project

7,687 Views
koehlerl
Contributor IV

Hi,

I created a project with SDK 0.85. Now I installed the latest update 3 with SDK. 0.86 and  processor expert update.

I changed the SDK from 0.85 to 0.86.

Now I have the problem, that all the components I had defined in the PE are missing.

BR Lutz

Labels (1)
0 Kudos
Reply
6 Replies

6,486 Views
koehlerl
Contributor IV

Hi Rares,

I have a other Window for change PE path ?

Wich S32DS version do you use?

PE_Path_select.png

0 Kudos
Reply

6,486 Views
raresvasile
NXP Employee
NXP Employee

Hi Lutz,

One workaround would be to disable older SDK repositories from Window->Preferences->Processor Expert-> Repositiories and Paths and then import the components as described in the post above.

pastedImage_1.png

Some of the component properties types have changed from one release to another and will require reconfiguration.

At which time the files from the repository are copied to the project SDK path?

Can you provide more details regarding this question?

Where can I find the sCST lib ?

sCST component can be added in the project as a usual PEx component and it will link the required files in the project.

Also you can find it in <sdk path>/lib/S32K14x/sCST

Best regards,

Rares

0 Kudos
Reply

6,484 Views
koehlerl
Contributor IV

Hi,

I have imported my PE configuration, but now I have a problem with the with the UART Baudrate.

PE don’t except my baudrate.

It’s the only component witch has a problem.

BR

Lutz

Von: raresvasile

Gesendet: Mittwoch, 3. Januar 2018 10:02

An: Köhler, Lutz <lutz.koehler@acd-antriebstechnik.de>

Betreff: Re: - Re: Update SDK in a S32DS project

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Update SDK in a S32DS project

reply from Rares Vasile<https://community.nxp.com/people/raresvasile?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/974123?commentID=974123&et=watches.email.thread#comment-974123>

0 Kudos
Reply

6,483 Views
jiri_kral
NXP Employee
NXP Employee

Hi Lutz, 

here is workaround  - before switching workspace you can export processor expert settings and after workspace update import it. 

Jiri

0 Kudos
Reply

6,480 Views
koehlerl
Contributor IV

Hi Jiri,

when I use this workaround the components are use the “old” repository.

I want to use the new SDK with the old configurations from the components.

I tried to change the repository for the components separate, but then then configuration in the components changed.

Question:

At which time the files from the repository are copied to the project SDK path?

Where can I find the sCST lib ?

Lutz

Von: jiri.kral@nxp.com

Gesendet: Dienstag, 19. Dezember 2017 14:37

An: Köhler, Lutz <lutz.koehler@acd-antriebstechnik.de>

Betreff: Re: - Re: Update SDK in a S32DS project

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Update SDK in a S32DS project

reply from Jiri Kral<https://community.nxp.com/people/jiri.kral@nxp.com?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/971279?commentID=971279&et=watches.email.thread#comment-971279>

0 Kudos
Reply

6,480 Views
jiri_kral
NXP Employee
NXP Employee

Hi Lutz, 

Thanks for report. I can confirm that some components disappear after project migration from  SDK v0.8.5 to v 0.8.6 - for example lpuart. I forwarded your question to SDK team - hope they will sahare more details. 

Jiri 

0 Kudos
Reply