Unable to use RTD in S32DS 3.6.1 on Linux – Missing headers (Platform_Types.h, pwm.h)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to use RTD in S32DS 3.6.1 on Linux – Missing headers (Platform_Types.h, pwm.h)

583 次查看
leojfrancis
Contributor I

I’m using S32DS 3.6.1 on Linux. The installation of S32DS itself was successful, and I was able to install the development package without issues.

However, when I tried to install RTD via HelpInstall New Software, I selected the RTD package for my target controller family and completed the installation.

After installation, I didn’t see the RTD plugin listed in the Plugins menu, but I was able to create a project from an example. I also found the RTD files and manuals in the software folder within the installation directory, so I assumed the installation was successful.

The problem is: when I try to build the example (a simple PWM test), the compiler fails with errors like:

13:08:25 **** Build of configuration Debug_FLASH for project Pwm_example_S32K344 ****

make -j16 all

Building file: ../src/main.c

Building file: ../Project_Settings/Startup_Code/exceptions.c

Invoking: Standard S32DS C Compiler

arm-none-eabi-gcc "@src/main.args" -MMD -MP -MF"src/main.d" -MT"src/main.o" -o "src/main.o" "../src/main.c"

Invoking: Standard S32DS C Compiler

arm-none-eabi-gcc "@Project_Settings/Startup_Code/exceptions.args" -MMD -MP -MF"Project_Settings/Startup_Code/exceptions.d" -MT"Project_Settings/Startup_Code/exceptions.o" -o "Project_Settings/Startup_Code/exceptions.o" "../Project_Settings/Startup_Code/exceptions.c"

Building file: ../Project_Settings/Startup_Code/system.c

Invoking: Standard S32DS C Compiler

arm-none-eabi-gcc "@Project_Settings/Startup_Code/exceptions.args" -MMD -MP -MF"Project_Settings/Startup_Code/system.d" -MT"Project_Settings/Startup_Code/system.o" -o "Project_Settings/Startup_Code/system.o" "../Project_Settings/Startup_Code/system.c"

../src/main.c:26:10: fatal error: Pwm.h: No such file or directory

26 | #include "Pwm.h"

| ^~~~~~~

../Project_Settings/Startup_Code/exceptions.c:40:10: fatal error: Platform_Types.h: No such file or directory

40 | #include "Platform_Types.h"

| ^~~~~~~~~~~~~~~~~~

../Project_Settings/Startup_Code/system.c:46:10: fatal error: Platform_Types.h: No such file or directory

46 | #include "Platform_Types.h"

| ^~~~~~~~~~~~~~~~~~

compilation terminated.

compilation terminated.

compilation terminated.

make: *** [Project_Settings/Startup_Code/subdir.mk:42: Project_Settings/Startup_Code/system.o] Error 1

make: *** Waiting for unfinished jobs....

make: *** [Project_Settings/Startup_Code/subdir.mk:42: Project_Settings/Startup_Code/exceptions.o] Error 1

make: *** [src/subdir.mk:20: src/main.o] Error 1

"make -j16 all" terminated with exit code 2. Build might be incomplete.

 

13:08:25 Build Failed. 7 errors, 0 warnings. (took 292ms)

It seems the SDK isn’t being found or linked properly. Has anyone encountered this issue before? How can I fix this so the project compiles correctly?

标签 (1)
0 项奖励
回复
0 回复数