USB_OTG device debugging issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB_OTG device debugging issues

2,512件の閲覧回数
1692470640
Contributor I

In debugging the USB device, I encountered the following problems:
1, the first time i receive the setup package, there is no UI interruption, even though I have configured the ios in dQH, and enabled the UE bit  in the UOTG_USBINTR. So I can only handle it by queryating at the moment.
2, in response to the host's first request (get the length bit 64 bytes of device descriptor), when I configure dQH and dTD and prime endpoint 0, will always enter the system error interrupt.
Please solve the problem for me, thank you!

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,390件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you please specify about which device are you talking?

regards,

Peter

0 件の賞賛
返信

2,390件の閲覧回数
1692470640
Contributor I

Hello Peter,

I used the devkit-mpc5748g development board.

thanks!

0 件の賞賛
返信

2,390件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I have moved this thread to SDK as the USB driver is part of SDK.

regards,

Peter

0 件の賞賛
返信