There is an error in the EB tresos clock configuration.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

There is an error in the EB tresos clock configuration.

1,447 Views
harryoceana
Contributor II

   The hardware uses a 25M passive crystal oscillator. When configuring EB tresos, it gives a clock prompt indicating that the frequency is out of range. Is this a configuration error on my part or a bug in EB tresos itself? How should I solve this problem?

 

harryoceana_0-1754062649013.png

harryoceana_1-1754062843391.pngharryoceana_2-1754062892089.png

It is allowed in S32DS.

harryoceana_3-1754062969369.png

 

 

 

Labels (1)
0 Kudos
Reply
5 Replies

1,376 Views
harryoceana
Contributor II

harryoceana_0-1754633487238.png

Using version 6.0.0 of RTD, this error still exists.   SW32K3_S32M27x_RTD_R21-11_6.0.0_D2506

0 Kudos
Reply

1,367 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @harryoceana 

To rule out issues caused by missing or incorrect configurations, you can use the Im- and Exporters... in EB Tresos to import the configuration from S32DS. Please refer to the following thread for detailed steps.

Tresos computes the wrong QSPI_SFCK_CLK clock frequency

0 Kudos
Reply

1,428 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @harryoceana 

To analyze the problem, could you please let me know which specific RTD version and Tresos Studio version you are using?

 

BR, VaneB

0 Kudos
Reply

1,388 Views
harryoceana
Contributor II

RTD version:SW32K3_RTD_R21-11_3.0.0_P07_D2306

Tresos Studio version: 29.0

0 Kudos
Reply

1,384 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @harryoceana 

We highly recommend updating to the latest software and tool versions. Each release includes important bug fixes and improvements that enhance stability and functionality.

0 Kudos
Reply