SDK required although I installed the latest version of SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK required although I installed the latest version of SDK

4,990件の閲覧回数
abderrahimjamao
Contributor III

Hello, I have a problem when I try to install an existing project.

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

4,723件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

The MTRDEVKSBNK144 example code is built on an older SDK EAR 0.8.6 which is not supported by the new S32DS for AMR v 2.2. Because between the SDK versions are differences the easiest way will be to use the S32DS for ARM v 2018.R1. It is possible to import and run this example code to the S32DS for ARM v 2018.R1 with a few changes in the properties. S32 Design Studio IDE for Arm® based MCUs | NXP 

This question have been discussed here:

https://community.nxp.com/message/1278208 

I hope it helps.

Best regards,

Diana

0 件の賞賛
返信

4,723件の閲覧回数
abderrahimjamao
Contributor III

ok, thank you so much. 

0 件の賞賛
返信

4,723件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

If you will have any difficulties with importing MTRDEVKSBNK144 to S32DS ARM v 2018.R1, please, let me know.

Best regards,

Diana

0 件の賞賛
返信

4,723件の閲覧回数
abderrahimjamao
Contributor III

Thank you very much I managed to import the project but I have an error when I debug the project.debug.PNG

0 件の賞賛
返信

4,723件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

What happens when you click the "Retry" button?

Are you able to build the project without any error?

May I see your debug configuration?

For example, I'm using OpenSDA so my settings see below:

pastedImage_2.png

Best regards,

Diana

0 件の賞賛
返信

4,723件の閲覧回数
abderrahimjamao
Contributor III

thankyou, it was a bad contact between the shield and the board. 

0 件の賞賛
返信