SDK in zip where to download

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK in zip where to download

2,262件の閲覧回数
axdwqerf
NXP Employee
NXP Employee

Hi, 

I would like to use the S32 SDK (S32_SDK_S32K1xx_RTM_4.0.3). See from the previous thread that I need to download the .zip file instead of .exe which will be easier to add in S32DS.

Where can I download the S32_SDK_S32K1xx_RTM_4.0.3.zip ??

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,190件の閲覧回数
Franky31
Contributor I

Exact same question here. I'm using S32DS 2018.R1 for years. I want to upgrade to v3.6.0, But I'm not able to find the latest S32 SDK in zip format. I installed the exe version, but it does not seem to be usable in S32DS. 

Why doesn't the zip version appear in the download area ?

 

Thanks for supporting

Franck

0 件の賞賛
返信

2,232件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi chinghsuan,

I have sent an email to you.

BR, Petr

0 件の賞賛
返信

1,500件の閲覧回数
dylan_yumq
Contributor I

Can I have a copy

0 件の賞賛
返信