SDK in zip where to download

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDK in zip where to download

2,261 次查看
axdwqerf
NXP Employee
NXP Employee

Hi, 

I would like to use the S32 SDK (S32_SDK_S32K1xx_RTM_4.0.3). See from the previous thread that I need to download the .zip file instead of .exe which will be easier to add in S32DS.

Where can I download the S32_SDK_S32K1xx_RTM_4.0.3.zip ??

标签 (1)
0 项奖励
回复
3 回复数

1,189 次查看
Franky31
Contributor I

Exact same question here. I'm using S32DS 2018.R1 for years. I want to upgrade to v3.6.0, But I'm not able to find the latest S32 SDK in zip format. I installed the exe version, but it does not seem to be usable in S32DS. 

Why doesn't the zip version appear in the download area ?

 

Thanks for supporting

Franck

0 项奖励
回复

2,231 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi chinghsuan,

I have sent an email to you.

BR, Petr

0 项奖励
回复

1,499 次查看
dylan_yumq
Contributor I

Can I have a copy

0 项奖励
回复