SDK Installation error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK Installation error

2,089件の閲覧回数
m15271429467
Contributor I

Thanks for your attention. After installing S32 Design studio, I tried to install the downloaded SDK package(S32DS_ARM_v2018.R1_UP10) through the following steps( help--> install new software--> S32DS_ARM_v2018.R1_UP10), but there was an installation error, the specific error message is shown in the figure.How to solve problem? Thank you!

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,951件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

from your screenshots it seems, that you are using S32DS v3.1 (or S32DS for Vision). The S32DS_ARM_v2018.R1_UP10 is not compatible with these versions. Please install correct S32DS version 

https://community.nxp.com/docs/DOC-340190 

Jiri

0 件の賞賛
返信

1,951件の閲覧回数
m15271429467
Contributor I

Thanks, already solve the problem.

发自我的 iPhone

在 2019年6月24日,下午5:34,jiri.kral@nxp.com <admin@community.nxp.com> 写道:

NXP Community

Re: SDK Installation error

reply from Jiri Kral in S32 SDK - View the full discussion

Hi,

from your screenshots it seems, that you are using S32DS v3.1 (or S32DS for Vision). The S32DS_ARM_v2018.R1_UP10 is not compatible with these versions. Please install correct S32DS version

S32 Design Studio for ARM 2018.R1 (Windows/Linux) released!

Jiri

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in S32 SDK by email or at NXP Community

Following Re: SDK Installation error in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

>

0 件の賞賛
返信

1,951件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

Can you please clarify which version of S32DS do you use?

This update is for the S32 Design Studio for Arm 2018.R1:

S32 Design Studio IDE for Arm® based MCUs | NXP 

Best Regards,

Diana

0 件の賞賛
返信