S32K148 PDB ADC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K148 PDB ADC

跳至解决方案
2,998 次查看
QJ_HAPPY
Contributor I

HI:

When I configure the BACK-TO-BACK mode of PDB, can I only configure channels 0-7 in sequence, but not remove channels from the middle ?

Thanks

 

标签 (1)
0 项奖励
回复
1 解答
2,993 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please read the "46.1.3 Back-to-back acknowledgement connections" and "Figure 46-5. PDB-ADC back to back con": Back-to-back operation enables the ADC conversions complete to trigger the next PDB channel pre-trigger and trigger output.

Back-to-back acknowledgement connections.png

There is no such possibility that Pre-trigger 0 COCO is directly connected to Pre-trigger 2.

Figure 46-5. PDB-ADC back to back connection.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,994 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please read the "46.1.3 Back-to-back acknowledgement connections" and "Figure 46-5. PDB-ADC back to back con": Back-to-back operation enables the ADC conversions complete to trigger the next PDB channel pre-trigger and trigger output.

Back-to-back acknowledgement connections.png

There is no such possibility that Pre-trigger 0 COCO is directly connected to Pre-trigger 2.

Figure 46-5. PDB-ADC back to back connection.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,985 次查看
QJ_HAPPY
Contributor I
I understand now. Thank you for your reply
0 项奖励
回复