S32K1 using Lpit to periodically trigger ADC using RTDs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K1 using Lpit to periodically trigger ADC using RTDs

ソリューションへジャンプ
3,839件の閲覧回数
hns80
Senior Contributor I

I'm having trouble modifying the Adc_Pdb_Ip example to trigger the ADC from the LPIT.

I'm not sure what I'm missing. I tried looking at the older examples using the SDK and don't see anything missing from what I'm doing with the RTDs.

My project is attached. What do I need to change to get the lpit to trigger the ADC conversion?

 

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
3,799件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

should the LPIT trigger PDB-ADC? As the example sets the PDB too and by default ADC is set to be triggered from PDB. There is check box "Enable SIM ADC source selections" in ADC component which allows you to change HW trigger to be done from TRGMUX (LPIT).
So if LPIT-PDB-ADC sync should be done then TRGMUX should be set to have 

PetrS_0-1652792413504.png

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,800件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

should the LPIT trigger PDB-ADC? As the example sets the PDB too and by default ADC is set to be triggered from PDB. There is check box "Enable SIM ADC source selections" in ADC component which allows you to change HW trigger to be done from TRGMUX (LPIT).
So if LPIT-PDB-ADC sync should be done then TRGMUX should be set to have 

PetrS_0-1652792413504.png

BR, Petr

0 件の賞賛
返信
3,763件の閲覧回数
hns80
Senior Contributor I

I used the tips you provided to make the example work as intended. It now triggers the ADC conversion every 10ms.

I attached the sample project in case anyone wants to see a sample implementation

0 件の賞賛
返信