[S32DS] `.project` buggy

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[S32DS] `.project` buggy

557 次查看
CY9
Contributor III

as the title 

CY9_0-1759280216858.pngCY9_1-1759280228168.png

 

in file '.project' :

CY9_2-1759280369873.png

 

 

#S32DS S32DS-S32PLATFORM #RTM402  S32DS-ARM 

标签 (1)
标记 (3)
0 项奖励
回复
5 回复数

534 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @CY9,

The SDK release notes specify the compatible IDE version.

S32SDK_for_S32K1xx_RTM_4.0.2_ReleaseNotes.pdf

danielmartynek_1-1759304933708.png

 

 

BR, Daniel

0 项奖励
回复

415 次查看
CY9
Contributor III
I don't think this is the root cause.


If you're right ...
(In this case, )
Why does it *ONLY* happen with `adc_driver.dox`?
Why does it *NOT* happen with `osif.dox` before it and `clock_manager.dox` after it?

This happens with different .dox files in different projects, (and it always happens with the .dox file?).
0 项奖励
回复

388 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @CY9,

It does not matter that the issue only occurs with the files only. In general, NXP does not guarantee the SDK functionality when used with incompatible software. Even if we resolve this particular issue, similar problems may arise later. To ensure a stable environment, please start with a fresh installation of S32DS 3.4 and install only SDK 4.0.2 — do not include any other SDKs or RTDs.

 

Regards,

Daniel

 

 

0 项奖励
回复

385 次查看
CY9
Contributor III

Wouldn't you recommend installing version 3.5 directly? 

 

Also, is it not recommended to install SDK4.0.1 at the same time?
Just install 4.0.2 ONLY ? 

0 项奖励
回复

380 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

S32DS 3.4 is compatible with the SDK not 3.5.

If you want 3.5 or the newest 3.6, use it with a compatible S32K1xx RTD.

In general, yes, it is better to have just one SDK/RTD per an IDE installation.

You can have more S32DS installations.

 

Regards,

Daniel

 

0 项奖励
回复