[S32DS] `.project` buggy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[S32DS] `.project` buggy

570 Views
CY9
Contributor III

as the title 

CY9_0-1759280216858.pngCY9_1-1759280228168.png

 

in file '.project' :

CY9_2-1759280369873.png

 

 

#S32DS S32DS-S32PLATFORM #RTM402  S32DS-ARM 

Labels (1)
0 Kudos
Reply
5 Replies

547 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @CY9,

The SDK release notes specify the compatible IDE version.

S32SDK_for_S32K1xx_RTM_4.0.2_ReleaseNotes.pdf

danielmartynek_1-1759304933708.png

 

 

BR, Daniel

0 Kudos
Reply

428 Views
CY9
Contributor III
I don't think this is the root cause.


If you're right ...
(In this case, )
Why does it *ONLY* happen with `adc_driver.dox`?
Why does it *NOT* happen with `osif.dox` before it and `clock_manager.dox` after it?

This happens with different .dox files in different projects, (and it always happens with the .dox file?).
0 Kudos
Reply

401 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @CY9,

It does not matter that the issue only occurs with the files only. In general, NXP does not guarantee the SDK functionality when used with incompatible software. Even if we resolve this particular issue, similar problems may arise later. To ensure a stable environment, please start with a fresh installation of S32DS 3.4 and install only SDK 4.0.2 — do not include any other SDKs or RTDs.

 

Regards,

Daniel

 

 

0 Kudos
Reply

398 Views
CY9
Contributor III

Wouldn't you recommend installing version 3.5 directly? 

 

Also, is it not recommended to install SDK4.0.1 at the same time?
Just install 4.0.2 ONLY ? 

0 Kudos
Reply

393 Views
danielmartynek
NXP TechSupport
NXP TechSupport

S32DS 3.4 is compatible with the SDK not 3.5.

If you want 3.5 or the newest 3.6, use it with a compatible S32K1xx RTD.

In general, yes, it is better to have just one SDK/RTD per an IDE installation.

You can have more S32DS installations.

 

Regards,

Daniel

 

0 Kudos
Reply