S32DS parallel Peripheral configuration in one project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS parallel Peripheral configuration in one project

跳至解决方案
4,463 次查看
abemat
Contributor III

In my project I am targetting two hardware revisions from within the project. The revisions differ slightly in code, but also in pin out and peripheral configuration.

Therefore, I need to be able to have multiple pin configurations and peripheral configurations. I succeeded in doing this for pin configurations, but for peripheral configurations I am having a harder time. The unsuccesfull steps I follow are these:

1. Go to "Peripherals" view

2. Open "Functional Group Properties"

3. Add new "Functional Group". This creates a new option to select in the "Functional Groups" drop down. Both options result in the same "Drivers" being shown (see below for the same view for both groups)

abemat_0-1665570402497.png

4. When I remove a driver, it is removed for both Functional Groups, whereas I only want it removed for the Functional Group under change. How can I make this possible?

In the end I would like to achieve two parallel Functional Groups which both configure eMios instance 1, but with different parameters.

 

 

 

 

标记 (5)
0 项奖励
回复
1 解答
4,138 次查看
namnguyenviet
NXP Employee
NXP Employee

Hello @abemat 

I don't know whether the issue is still persist in your site, but from my site with the following environment:

S32 Design Studio for S32 Platform, Version: 3.4, Build id: 201217 (Update 3)

S32K3 Development Package, version 3.4.3

S32K3 RTD 2.0.0

I was able to add a module in just one function group, while the others are not.

Best Regards,

Nam

在原帖中查看解决方案

0 项奖励
回复
6 回复数
4,139 次查看
namnguyenviet
NXP Employee
NXP Employee

Hello @abemat 

I don't know whether the issue is still persist in your site, but from my site with the following environment:

S32 Design Studio for S32 Platform, Version: 3.4, Build id: 201217 (Update 3)

S32K3 Development Package, version 3.4.3

S32K3 RTD 2.0.0

I was able to add a module in just one function group, while the others are not.

Best Regards,

Nam

0 项奖励
回复
4,120 次查看
abemat
Contributor III

Hi Nam,

Thanks for getting back to us. When trying again - also with S32DS Version: 3.4 Build id: 201217 (Update 3) - it seems to work for me. I can add/duplicate a new function group, and can add/alter configurations. Even though I am not planning to use this feature anymore, I believe this is what I would want.

However, I think my initial misunderstandig of its function was that when I remove any of the elements in the left "Components" view, they will be removed from all Function Groups, not only the one currently active. However, I now realize this is more of a UI/UX misunderstanding than functional issue.

abemat_0-1681200790733.png

 

0 项奖励
回复
4,423 次查看
gpira
Contributor III

Sorry if I jump in but I have a similar problem and I'm looking for an answer.

I'm trying to create two different pin configurations in a single project, you said you manage to do that, how?

Did you create 2 different Pin Functional Groups? Do you think it is doable also with two different packages (64 pin and 100 pin).

Thanks

0 项奖励
回复
4,419 次查看
abemat
Contributor III

Yep, I created more than two different pin Functional Groups and only initialize the ones required.

I have no experience with setting them up for different packages. To use the Pin ConfigTool in S32DS you first have to specify your package - or when changing, respecify your package - so sadly for you, I have little hope different packages are supported simultaneously in a single S32DS project.

You could also create a separate dummy project for the other package, update your pinconfig over there, and only include the desired pinconfig depending on your build target.

4,437 次查看
abemat
Contributor III

Any update on this? @davidtosenovjan @jiri_kral 

0 项奖励
回复
4,371 次查看
abemat
Contributor III

bump?

标记 (1)
0 项奖励
回复