S32DS examples compile issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS examples compile issue

4,795件の閲覧回数
weisenzhang
Contributor I

hi, 

I have problem on compiling when imported the examples.

here is my log:

arm-none-eabi-gcc -DCPU_S32K144HFT0VLLT -DS32K -I"E:\workspace\FreeRTOS_Example\Sources" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/examples/demo_apps/FreeRTOS/sources" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/rtos/FreeRTOS/Source/include" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/rtos/FreeRTOS/Source/portable/MemMang" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/rtos/FreeRTOS/Source/portable/GCC/ARM_CM4F" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/platform/devices/S32K144/include" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/platform/devices/S32K144" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/platform/devices" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/platform/hal/inc" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/platform/drivers/inc" -O0 -g3 -Wall -c -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -mcpu=cortex-m4 -mthumb -mfloat-abi=softfp -mfpu=fpv4-sp-d16 -specs=nano.specs -specs=nosys.specs --sysroot="D:\Freescale\S32_ARM_v1.2\eclipse\../Cross_Tools/gcc-arm-none-eabi-4_9/arm-none-eabi/newlib" -MMD -MP -MF"Sources/main.d" -MT"Sources/main.o" -c -o "Sources/main.o" "../Sources/main.c"
../Sources/main.c:61:17: fatal error: Cpu.h: No such file or directory
#include "Cpu.h"

ラベル(1)
3 返答(返信)

3,765件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello,

It seems like generated files from Processor Expert do not exist.

I'd recommend you to generate the processor expert code first since build process does not trigger the code generator.

 pastedImage_3.png

When the generation is done you should see the new project folder "Generated Code" which includes e.g. "cpu.h" that was missing when you initially compiled main.c.

Now you can build the project and at the end of the process you should see executable elf file being created:

pastedImage_4.png

Hope it helps.

Stan

3,765件の閲覧回数
taehokwon
Contributor I

Thanks.

0 件の賞賛
返信

3,765件の閲覧回数
weisenzhang
Contributor I

thanks, Stan, that's right, it works now.

0 件の賞賛
返信