S32 SDK EAR 0.8.6 version download error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 SDK EAR 0.8.6 version download error

Jump to solution
3,727 Views
HeeSu
Contributor I

Hi Sir,

I'm using the S32K148EVB board with the "S32DS for ARM" IDE. 

I'd like to download the EAR 0.8.6 SDK on Windows 10.


However, the installation could not be completed for some reason.

I downloaded the archive file from NXP site but it not working.

Is there any problem my process?

 

Best,

 

HeeSu_0-1679958911446.png

 

 

 

Labels (1)
0 Kudos
Reply
1 Solution
1,526 Views
Robin_Shen
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
3 Replies
3,710 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

S32 SDK 0.8.6 EAR is available in S32DS_ARM_v2018.R1 or S32 Design Studio for Arm v2.0 - Update 3 available.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,949 Views
HeeSu
Contributor I

Hi @Robin_Shen 

First Link you gave me S32DS_ARM v2018.R1 is expired, I can not download it.

I followed the process written on the second Link but still not working.

HeeSu_0-1679970231253.png

 

0 Kudos
Reply
1,527 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please try this link: https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-ARM-2018-R1-Wind...(Fully integrated S32 SDK for S32K14x EAR release v.0.8.6.)

0 Kudos
Reply