S32 Design Studio: How to upgrade SDK version of an existing project?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Design Studio: How to upgrade SDK version of an existing project?

2,098 次查看
sripav-7
Contributor III

Hello

I have an existing project developed using the EAR 0.8.6 SDK and I would like to upgrade it to 1.9.0 BETA SDK but can't figure out a way to do it. Can someone please guide me through?

Thank you

标记 (4)
1 回复

1,721 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

these versions aren't fully compatible. You can try export PE settings, but some module you will need to configure manually. The only 100% working solution is create  new project with SDK you are interested in, add your sources and create new Processor Expert settings. 

I recommend you use SDK v2.0 RTM instead the 1.9 beta. 

Jiri