S32 Design Studio: How to upgrade SDK version of an existing project?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio: How to upgrade SDK version of an existing project?

2,095件の閲覧回数
sripav-7
Contributor III

Hello

I have an existing project developed using the EAR 0.8.6 SDK and I would like to upgrade it to 1.9.0 BETA SDK but can't figure out a way to do it. Can someone please guide me through?

Thank you

タグ(4)
1 返信

1,718件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

these versions aren't fully compatible. You can try export PE settings, but some module you will need to configure manually. The only 100% working solution is create  new project with SDK you are interested in, add your sources and create new Processor Expert settings. 

I recommend you use SDK v2.0 RTM instead the 1.9 beta. 

Jiri