Regarding Restart a process

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding Restart a process

1,112 次查看
leekate-b45752
NXP Employee
NXP Employee

Hello, 

When I use SDK examples with debug_ram, the error occurred and the code didn't implement normally after RESTART as below, could you explain about this symptom? Is it normal behavior?

pastedImage_1.png

pastedImage_2.png

Best regards,

Kate Lee

标签 (1)
0 项奖励
回复
1 回复

1,051 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Kate, 

This behavior is due to the PEmicro firmware that all the EVBs have. When you click the restart button on the IDE the debugger is restarting the MCU hence you are losing the program since it's in RAM. As a workaround, you could change the firmware of the on-board debugger to JLink instead of PEmicro. The JLink debug configurations have an option to make the restart works even if you are running from RAM. pastedImage_1.png

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------- 

0 项奖励
回复