Hi,
I want to rebulid kernel like csi.o, and while reading VisionSDK_S32V2_RTM_1_3_0 user guide. Some questions occurred at 3.3.1 and 3.3.2.
3.3.1General Preparation
o export LINUX_S32V234_DIR=/linux/sources/directory/for/s32v234/
optional, only for s32v234 Linux build
Path to the Linux sources (same kernel as is running on the board)
o export PATH=/path/to/your/compiler/binaries:$PATH
Path to the compiler binaries
I can't find "linux sources" directory in VisionSDK_S32V2_RTM_1_3_0 folders. And if I try to run "make allsub" on Windows via msys32 in "VisionSDK_S32V2_RTM_1_3_0\s32v234_sdk\libs\isp\csi\kernel\build-v234ce-gnu-linux-d",
I got this: Makefile:81: *** Please define LINUX_S32V234_DIR pointing to kernel directory
@bpe
Please be aware, that support to S32V234 Vision subsystem modules is done only
via tickets. This Community is not appropriate for questions of this kind. I
will contact you by e-Mail with respect to this issue, for future requests,
please:
1. Register yourself on NXP Website with your corporate e-Mail.
2. Use tickets to submit questions.
Have a great day,
Platon
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------